MLFB_PlsPosFwBw

Pipe Network motion icon

 Function Block - Forward/backward position range indicator.

Inputs

Input

Data Type

Range

Unit

Default

Description

ibExecute

BOOL

 

 

 

 

 

 

Enable PLS.

iAnyModuloBlkID

DINT

 

 

 

 

 

 

Any modulo pipe network block ID.

iStartPos

LREAL

 

 

 

 

 

 

Start position of PLS.

iEndPos

LREAL

 

 

 

 

 

 

End position of PLS.

iDelayTime

TIME

 

 

 

 

 

 

Delay time for compensation.

iHysteresis

LREAL

 

 

 

 

 

 

Hysteresis.

ibForce

BOOL

 

 

 

 

 

 

Force PLS.

Outputs

Output

Data Type

Range

Unit

Description

oPLS

BOOL

 

 

N/A

Position limit switch.

Remarks

  • Used in the command or actual position path, e.g., sampler pipe with noisy position, in both directions.
  • Any modulo pipe block is needed, which can also be used for another instance of this UDFB.
  • It is also possible to define a hysteresis for switching on and off of the PLS.
  • The Boolean output oPLS is set to:
    • TRUE if the position has crossed the start position.
    • FALSE if the position has crossed the end position.
  • The function block is executed cyclically.
    • The modulo position is considered.
  • The function block has the possibility to compensate a delay time of the connected device (e.g., glue nozzles).

Timing

Hysteresis

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//PLSOutput is True when chosen comparator is between 180 and 270 with a T#2ms delay

//Can also force the output to be true with ForceOuput variable

//Hysteresis is on for 3 user units in case direction changes around start point

Inst_MLFB_PlsPosFwBw( EnablePLS, PipeNetwork.COMPARATOR, 180, 270, T#2ms, 3, ForceOutput );
PLSOutput := Inst_MLFB_PlsPosFwBW.oPLS;