MC_GrpReadBoolPar
Function Block - Reads a value from the specified Boolean group parameter.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Enable |
BOOL |
FALSE, TRUE |
N/A |
No default |
If TRUE, then request to read a value from the specified Boolean group parameter. |
|
AxesGroupRef |
N/A |
N/A |
No default |
The axis group the Boolean parameter value is read from. |
|
|
ParamNum |
UINT |
1000, 1001 |
UINT |
No default |
ParamNum can be one of these two defined Booleans:
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Done |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the command completed successfully. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
INT |
No range |
N/A |
Indicates the error if Error output is TRUE. |
|
ParamValue |
BOOL |
FALSE, TRUE |
N/A |
TRUE or FALSE. |
Remarks
-
-
This function or function block returns cached data.
See Program a Multi-Core Controller.
- See Coordinated Motion, the top-level topic for Coordinated Motion.
- See Function Blocks - General Rules about how inputs and outputs work.
- See Recovery of the System State After an Axis Error.
- MC_GrpReadBoolPar(Axesgroup_Ref GroupID, Uint BoolID) where BoolID can be one of these two currently defined Booleans:
- IGNORE_AXIS_ESTOP:
- ID = 1000
- The value read is either TRUE or False as set by the MC_GrpWriteBoolPar function block.
- AXIS_ESTOP_ACTIVE:
- ID = 1001
- This read-only parameter is asserted TRUE whenever an axis in the group is experiencing an Axis Estop Error.
- When there are no Axis Estop Errors present on the axes in a group, this parameter is set to FALSE.
- IGNORE_AXIS_ESTOP:
Figure 1: MC_GrpReadBoolPar
FBD Language Example
FFLD Language Example
IL Language Example
BEGIN_IL
Cal Inst_GrpReadBoolPar( DoEnable, Group1_Ref, AXIS_ESTOP_ACTIVE )
END_IL
ST Language Example
Inst_GrpReadBoolPar( DoEnable, Group1_Ref, AXIS_ESTOP_ACTIVE );
See Also