MC_UngroupAllAxes
Function Block - Removes all axes from an axes group.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Execute |
BOOL |
FALSE, TRUE |
N/A |
No default |
On the rising edge, request to remove all axes in the axes group. |
|
AxesGroupRef |
No range |
N/A |
No default |
The axis group from which to remove all axes. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Done |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the command completed successfully. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
INT |
Enumerated |
N/A |
Indicates the error if Error output is TRUE. |
Remarks
-
- This function block starts a motion-related action and stores data for calculations and error checking.
If using a dual-core controller, see Call Function Blocks Multiple Times in the Same Cycle.
- See Coordinated Motion, the top-level topic for Coordinated Motion.
- This function or function block does not generate any motion.
- This function block can be issued in the group states: (GroupDisabled, GroupStandby, or GroupErrorStop).
- The axes group state is changed to GroupDisabled upon successful completion.
- MC_UngroupAllAxes fails if the group is in any state other than GroupStandby or GroupDisabled.
- See Group State Diagrams.
Figure 1: MC_UngroupAllAxes
FBD Language Example
FFLD Language Example
IL Language Example
BEGIN_IL
CAL Inst_MC_UngroupAllAxes( ExecuteUngroup, Group1_Ref )
END_IL
ST Language Example
Inst_MC_UngroupAllAxes( ExecuteUngroup, Group1_Ref );
See Also