MC_GrpReadCmdPos
Function Block - Reads the command position of the axes in the group.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Enable |
BOOL |
FALSE, TRUE |
N/A |
No default |
If TRUE, this function block reads the current commanded position of the axes in the group. |
||||||||
|
AxesGroup |
No range |
N/A |
No default |
The axes group the commanded position is read from. |
|||||||||
|
CoordSystem |
SINT |
Enumerated |
N/A |
No default |
The coordinate system used when reading the commanded position. One of these enumeration values:
|
||||||||
|
Position |
LREAL[ ] |
Dimension: The number of axes in the AxesGroup. No range |
User units |
No default |
An array where the position data is written.
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Valid |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the positions have been read without error. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
INT |
No range |
N/A |
Indicates the error if Error output is TRUE. |
Remarks
-
-
This function or function block returns cached data.
See Program a Multi-Core Controller.
- See Coordinated Motion, the top-level topic for Coordinated Motion.
- See Function Blocks - General Rules about how inputs and outputs work.
- The MC_GrpReadCmdPos function block fills the array (specified by the
Positionargument) with the commanded position of the coordinate system specified by theCoordSystemargument. - This function or function block does not generate any motion.
-
-
Only the ACS coordinate system is supported.
See Coordinate Systems.
- There is a one-to-one correspondence between the axes in the Axes Group and the position values in the Position Array.
- Each element in the Position Array corresponds to the axis element in the Axis Group array.
- If an index in the Axes Group is unassigned, the position value for that array element in the Position Array is 0 (zero).
- If the element does contain an axis, the position value is filled with the current actual position for that axis.
Figure 1: MC_GrpReadCmdPos
FBD Language Example
FFLD Language Example
IL Language Example
BEGIN_IL
CAL Inst_MC_GrpReadCmdPos( DoRead, Group, CoordSys, PosList )
END_IL
ST Language Example
(*MC_GrpReadCmdPos ST example *)
Inst_MC_GrpReadCmdPos(DoRead, Group, CoordSys, PosList );
See Also