MLAxisGenWriteSpd

Pipe Network motion icon

 Function - Sets the speed of the internal generator of an axis.

Inputs

Input

Data Type

Range

Unit

Default

Description

AxisID

DINT

No range

N/A

No default

ID Name of the Axis block.

Speed

LREAL

No range

User unit/sec

No default

Sets the generator Speed value.

See Set the Axis Block Position Units.

Outputs

Output

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Returns TRUE when the function successfully executes.

See Function - General Rules.

Remarks

This function or function block does not generate any motion.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

 MLAxisGenWriteSpd(PipeNetwork.Axis1, 500 )  ;

See Also