MLAxisIsCnctd

Pipe Network motion icon

 Function - Verifies if a pipe is currently connected to the axis.

Inputs

Input

Data Type

Range

Unit

Default

Description

ID

DINT

No range

N/A

No default

ID Name of the Axis block.

Outputs

Output

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Returns TRUE when the function successfully executes.

See Function - General Rules.

Remarks

Returns TRUE if a pipe is connected.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

 MLAxisIsCnctd(PipeNetwork.Axis1 )  ;