MLAxisReadModPos

Pipe Network motion icon

 Function - Gets the value period of the axis.

Inputs

Input

Data Type

Range

Unit

Default

Description

AxisID

DINT

No range

N/A

No default

ID Name of the Axis block.

Outputs

Output

Data Type

Range

Unit

Description

OK

BOOL

FALSE, TRUE

N/A

Returns TRUE when the function successfully executes.

See Function - General Rules.

ModuloPosition

LREAL

 

User units

Returns the Axis Value Period.

Remarks

None

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Axis1_Value_Period := MLAxisReadModPos(PipeNetwork.Axis1 )  ;