MLAxisRstFastIn
Function - Writes in the Latch Control Word to reset the Fast Input.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
AxisID |
DINT |
No range |
N/A |
No default |
ID Name of the Axis block. |
|
InputID |
DINT |
No range |
N/A |
No default |
ID name of the Fast input of an axis (i.e., IN1 and IN2 on S300). InputID INT Range = 0, 1
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
Returns TRUE when the function successfully executes. See Function - General Rules. |
Remarks
None
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLAxisRstFastIn(PipeNetwork.Axis1, 0 ) ;
See Also