MLAxisWriteModPos

Pipe Network motion icon

 Function - Sets the value period of the axis.

Inputs

Input

Data Type

Range

Unit

Default

Description

AxisID

DINT

No range

N/A

No default

ID Name of the Axis block.

ModuloPosition

LREAL

No range

User units

No default

Sets the Axis Period Value when Mode is set to Modulo.

Outputs

Output

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Returns TRUE when the function successfully executes.

See Function - General Rules.

Remarks

None

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

 
MLAxisWriteModPos(PipeNetwork.Axis1, 360) ) ;