MLPmpForcePos
Function - Forces the position of a PMP block to a specified position.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
EN |
BOOL |
0, 1 |
N/A |
No default |
Enables execution. |
|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID name of a PMP function block in the Pipe Network. |
|
Position |
LREAL |
No range |
User units |
No default |
Defines the PMP starting position when the motion starts. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
|
N/A |
Returns TRUE when the function successfully executes. See Function - General Rules. |
Remarks
- This block can only be executed when motion is NOT occurring.
- It can be used to force the PMP starting position to the values to start motion from.
FBD Language Example
FFLD Language Example
-
-
A pulse contact is required to start the FB.
IL Language Example
Not available.
ST Language Example
MLPmpForcePos( PipeNetwork.PMP, 2500.0 );
See Also