MLSmpConnect
Function - Connects a sampler block to a pipe network axis or pipe block.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID Name of the SMP function block in the Pipe Network. |
|
PipeBlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID Name of the pipe block the sampler is connected to. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
|
N/A |
Returns TRUE if the Sampler is connected. See Function - General Rules. |
Remarks
None
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Connect a Sampler pipe block named “EncoderMaster1” to a PipeNetwork Axis block named AXIS1
MLSmpConnect( PipeNetwork.EncoderMaster1, PipeNetwork.AXIS1 ) ;
See Also