AND ANDN &
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
IN1 | BOOL | First Boolean input. | |||
IN2 | BOOL | Second Boolean input. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
BOOL |
|
|
Boolean AND of all inputs. |
Remarks
- In the FBD and FFLD languages, the block is called
&
.- To select the number, right-click on the block and choose the Set number of inputs command in the contextual menu.
- In ST and IL languages,
&
can be used instead of AND.
Truth Table
IN1 |
IN2 |
Q |
---|---|---|
0 |
0 |
0 |
0 |
1 |
0 |
1 |
0 |
0 |
1 |
1 |
1 |
FBD Language Example
- In the FBD Language, the block can have a maximum of 32 inputs.
FFLD Language Example
- In the FFLD Language, the block can have a maximum of 32 inputs.
IL Language Example
- In the IL Language, the AND instruction performs a logical AND between
the current result and the operand.
- The current result must be Boolean.
Op1: FFLD IN1
& IN2 (* "&" or "AND" can be used *)
ST Q (* Q is equal to: IN1 AND IN2 *)
Op2: FFLD IN1
AND IN2
&N IN3 (* "&N" or "ANDN" can be used *)
ST Q (* Q is equal to: IN1 AND IN2 AND (NOT IN3) *)
ST Language Example
Q := IN1 AND IN2;
Q := IN1 & IN2 & IN3;
See Also