DTSetNTPServer

 Function Block - Set the NTP server address.

This function block is specific for PCMM2G only.

Inputs

Input

Data Type

Range

Unit

Default

Description

Execute

BOOL

FALSE, TRUE

N/A

No default

If TRUE, request to set the NTP server address.

NTP Server

STRING

No range

N/A

No default

The address of the NTP server used for clock synchronization.

Outputs

Output

Data Type

Range

Unit

Description

Done

BOOL

FALSE, TRUE

N/A

If TRUE, the command completed successfully.

Error

BOOL

FALSE, TRUE

N/A

If TRUE, an error has occurred.

ErrorID

DINT

No range

N/A

Indicates the error if the Error output is set to TRUE.

Error Codes

  • 23 = Internal error.
    See the controller log for details.
  • 15000 = Controller type does not support this function block.

Remarks

None

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

// configure the NTP server address
Inst_DTSetNTPServer( bSetNTPServer, NTPServer );
if Inst_DTSetNTPServer.Done then
   bSetNTPServer := false;
   bError := Inst_DTSetNTPServer.Error;
   ErrorID := Inst_DTSetNTPServer.ErrorID;
end_if;

See Also