DTEvery
Function Block - Generate a pulse signal with long period.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Run |
BOOL |
FALSE, TRUE |
N/A |
No default |
When TRUE, the signal generation is enabled. |
|
Days |
DINT |
1 to 65536 |
Days |
No default |
Period : number of days. |
|
TM |
Time |
0 to 86,399,999 |
Milliseconds |
No default |
Rest of the period (if not a multiple of 24h). |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
BOOL |
FALSE, TRUE |
N/A |
Pulse signal. |
Remarks
- This function block provides a pulse signal with a period of more than 24h.
- The period
is expressed as:
DAYS * 24h + TM
- The period
is expressed as:
- Example: Specifying DAYS=1 and TM=6h means a period of 30 hours.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
(* MyDTEVERY is a declared instance of DTEVERY function block. *)
MyDTEVERY (RUN, DAYS, TM);
Q := MyDTEVERY.Q;
See Also