ScaleLin
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
IN |
REAL |
|
|
|
Real value. |
IMIN |
REAL |
|
|
|
Minimum input value. |
IMAX |
REAL |
|
|
|
Minimum input value. |
OMIN |
REAL |
|
|
|
Minimum output value. |
OMAX |
REAL |
|
|
|
Minimum output value. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
REAL |
|
|
Result: OMIN + IN * (OMAX - OMIN) / (IMAX - IMIN). |
Remarks
Truth Table
Inputs |
OUT |
---|---|
IMIN >= IMAX |
= IN |
IN < IMIN |
= OMIN |
IN > IMAX |
= OMAX |
other |
= OMIN + IN * (OMAX - OMIN) / (IMAX - IMIN) |
FBD Language Example
FFLD Language Example
- In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
- The output rung (ENO) keeps the same value as the input rung.
- The function is executed only if EN is TRUE.
- ENO keeps the same value as EN.
IL Language Example
- In the IL Language, the input must be loaded in the current result before calling the function.
Op1: LD IN
ScaleLin IMAX, IMIN, OMAX, OMIN
ST OUT
ST Language Example
OUT := ScaleLin (IN, IMIN, IMAX, OMIN, OMAX);