trunc / truncL
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
IN |
REAL / LREAL |
|
|
|
Real value. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
REAL / LREAL |
|
|
Result: Integer part of N. |
Remarks
None
FBD Language Example
FFLD Language Example
- In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
- The output rung (ENO) keeps the same value as the input rung.
- The function is executed only if EN is TRUE.
- ENO keeps the same value as EN.
IL Language Example
- In the IL Language, the input must be loaded in the current result before calling the function.
Op1: LD IN
TRUNC
ST Q (* Q is the integer part of IN *)
ST Language Example
Q := TRUNC (IN);
See Also