not_mask

PLCopen motion icon

 Function - Performs a bit-to-bit Boolean negation of an integer value.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

ANY

 

 

 

Integer input.

Outputs

Output

Data Type

Range

Unit

Description

Q

ANY

 

 

Bit to bit negation of the input.

Remarks

  • Arguments can be signed or unsigned integers from 8- to 32-bits.

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the input rung (EN) enables the operation.
    • The output rung keeps the state of the input rung.
    • The function is executed only if EN is TRUE.
    • ENO has the same value as EN.

IL Language Example

  • In the IL Language, the first parameter (IN) must be loaded in the current result before calling the function.
    • The other input is the operands of the function.
Op1: LD       IN
     NOT_MASK
     ST       Q

ST Language Example

Q := NOT_MASK (IN);

See Also