DEC

PLCopen motion icon

 Function - Decrease a numerical variable.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

ANY

 

 

 

Numerical variable (increased after call).

See FFLD Data In / Data Out for more information.

Outputs

Output

Data Type

Range

Unit

Description

Q

ANY

 

 

Decreased value.

Remarks

  • When the function is called, the variable connected to the IN input is decreased and copied to Q.
    • All data types are supported except BOOL and STRING.
      • For these types, the output is the copy of IN.
  • For real values, a variable is decreased by 1.0.
  • For time values, a variable is decreased by 1ms.
  • The IN input must be directly connected to a variable.
    • It cannot be a constant or complex expression.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

  • This function is particularly designed for the ST Language.
    • It allows simplified writing.
    • Assigning the result of the function is not mandatory.
IN := 2;
Q := DEC (IN);
(* now: IN = 1 ; Q = 1 *)
DEC (IN); (* simplified call *)