StringTable

PLCopen motion icon

 Function - Selects the active string table resource.

Inputs

Input

Data Type

Range

Unit

Default

Description

TABLE

STRING

 

 

 

Name of the Sting Table resource.

Must be a constant.

COL

STRING

 

 

 

Name of the column in the table.

Must be a constant.

Outputs

Output

Data Type

Range

Unit

Description

Q

BOOL

FALSE, TRUE

 

TRUE if OK.

Remarks

  • This function selects a column of a valid String Table resource to become the active string table.
    • The LoadString function always refers to the active string table.
  • Arguments must:
    • be constant string expressions.
    • fit to a declared string table and a valid column name within this table.
  • If there is only one string table with only one column defined in the project, you do not need to call this function.
    • It is the default string table.

FBD Language Example

FFLD Language Example

IL Language Example

Op1: LD
     'MyTable'
     StringTable 'First Column'
     ST
OK

ST Language Example

OK := StringTable ('MyTable', 'FirstColumn");

See Also