char

PLCopen motion icon

 Function - Builds a single character string.

Inputs

Input

Data Type

Range

Unit

Default

Description

CODE

DINT

 

 

 

ASCII code of the specified character.

Outputs

Output

Data Type

Range

Unit

Description

Q

STRING

 

 

STRING containing only the specified character.

Remarks

None

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the input rung (EN) enables the operation.
    • The output rung (ENO) keeps the same value as the input rung.

IL Language Example

  • In the IL Language, the input parameter (CODE) must be loaded in the current result before calling the function.
Op1: LD   CODE
     CHAR
     ST   Q

ST Language Example

Q := CHAR (CODE);

See Also

ascii