HToA

PLCopen motion icon

 Function - Converts and integer to a string using hexadecimal basis.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

DINT

 

 

 

Integer value.

Outputs

Output

Data Type

Range

Unit

Description

Q

STRING

 

 

String representing an integer in hexadecimal format.

Remarks

None

Truth Table

IN

Q

0

'0'

18

'12'

160

'A0'

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
    • The output rung (ENO) keeps the same value as the input rung.
    • The function is executed only if EN is TRUE.
    • ENO keeps the same value as EN.

IL Language Example

  • In the IL Language, the input must be loaded in the current result before calling the function.
Op1: LD  IN
     HTOA
     ST  Q

ST Language Example

Q := HTOA (IN);

See Also

AToH