FileReadLine
Function Block - Reads a string value from a text file.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Execute |
BOOL |
0, 1 |
N/A |
No default |
On the rising edge, read the size of a file. |
|
ID |
UDINT |
N/A |
N/A |
No default |
The ID of the open file. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Done |
BOOL |
|
|
If TRUE, the command completed successfully. |
|
Error |
BOOL |
|
|
If TRUE, an error has occurred. |
|
ErrorID |
DINT |
|
|
Indicates the error if Error output is TRUE. See the table in File and TCP/IP Function Block ErrorIDs. |
|
Value |
STRING |
|
|
The string value read from the file. |
Remarks
FileReadLine stops reading from the file if either:
- 255 characters are read (the maximum length of the STRING type).
- A new line is encountered.
Figure 1: FileReadLine
FBD Language Example
Not available.
FFLD Language Example
Not available.
IL Language Example
Not available.
ST Language Example
(* FileReadLine example *)
CASE StepCounter OF
0:
Inst_FileReadLine(TRUE, MyInputFileID);
StepCounter := StepCounter + 1;
1:
Inst_FileReadLine(TRUE, MyInputFileID);
IF Inst_FileReadLine.Done THEN
lineText := Inst_FileReadLine.Value;
Inst_FileReadLine(FALSE, 0);
StepCounter := StepCounter + 1;
END_IF;
END_CASE;
See Also