Motion Library

The Motion Library (ML) (for Pipe Network Concept and PLCopen®) is in the Function Blocks tab of the Library toolbox.

  • The KAS function library contains ML function blocks used to integrate motion in a PLC program.
  • ML function blocks can be used in four of the IEC 61131-3 languages: ST, FBD, FFLD and IL.
  • For Sequential Function Chart (SFC) programs, ML function blocks are used as part of SFC Steps or SFC Transitions defined with FBD, FFLD, IL, or ST languages.

Concept Link IconSee Also