Line-to-Arc and Arc-to-Line Transitions

With this transition mode, the linear move is shortened when one move is linear and the other is circular.

  • The amount is specified by the corner distance.
  • A circular arc connects the two moves, allowing for a smooth transition.
  • The circular arc that connects the two moves derives its velocity from the transition parameter and the acceleration and deceleration values are derived from the next move.

n-Degree Transition

Motion Path -
Line-to-Arc / Arc-to-Line

Key

Motion Velocity Profile

Blue: Incoming and outgoing linear and circular motion.

Red: Transition arc.

  1. Original start / endpoint of linear move.
  2. Corner distance.

Special Case Transitions

These are the special cases for Line-to-Arc and Arc-to-Line transitions:

Intersection Transition

Tangent Transition

Zero-distance Transition