Line-to-Line Transitions

When both moves are linear, the current and next moves are shortened using this transition mode.

  • The amount is specified by the corner distance.
  • A circular arc connects the two moves, with exceptions.
  • The circular arc that connects the two moves derives its velocity from the transition parameter.
  • The acceleration and deceleration values are derived from the next move.

n-Degree: Transition

Motion Path - Line-to-Line

Key

Motion Velocity Profile

Blue: Incoming and outgoing linear motion.

Red: Transition arc.

  1. Original endpoint of the 1st move.
  2. Corner distance.

Special Case Transitions

These are the special cases for line-to-line transitions:

180-degree Transition

Zero-degree Transition

Zero-distance Transition