Error Handling Behavior

Two outputs deal with errors that can occur while executing a function block.

These outputs are defined as:

  • Error: The rising edge of Error informs you that an error occurred during the execution of the function block.
  • ErrorID: Error number.
  • Done, InVelocity, InGear, and InSync mean successful completion.
    • These signals are logically exclusive to Error.
  • Instance errors do not always result in an axis error.