Use Cam Profiles

Once defined (see "Create a CAM Profile"), you can associate a cam profile to a cam Pipe Block in the Pipe Network as follows:

  1. Right-click on the cam Pipe Block and select Properties in the menu
  2. In the Parameters tab, enter the profile's name

    Cam - Associate Profile to a Pipeblock

  3. Figure 1: Cam - Associate Profile to a Pipeblock



  • Separating the declaration of the cam Pipe Block from the cam profile provides the capability to prepare several different cam profiles and then apply one of them to the cam Pipe Block.



  • If you change the profile's filename, do not forget to update the cam Pipe Block accordingly.