Cam Profile Segment Overview

Line Segment Type

Segment Curve

Velocity

Acceleration

Jerk

Supported by

KAS-IDE Profile Editor

MLProfileBuild

Continuous Velocity

Continuous Acceleration

Interpolation Method

Linear function: f(x) = Ax + B

Advantages

This segment type easily defines constant-velocity segments.

It can be used in very large numbers to define profiles of any size without having to specify the velocity or acceleration at the segment endpoints.

Disadvantages

Profiles can result in discontinuous velocities.

Parabolic Segment Type

Segment Curve

Velocity

Acceleration

Jerk

In the example:

  • The blue line represents the linear (constant velocity) part of the segment.
  • The black lines represent the parabolic (constant acceleration) parts of the segment.

Supported by

KAS-IDE Profile Editor

MLProfileBuild (parabolic option)

Continuous Velocity

Continuous Acceleration

Interpolation Method

Linear function: f(x) = Ax + B
2nd order polynomial: f(x) = Cx2 + Dx + E

Advantages

This segment type is used to define constant acceleration portions of a profile.

This minimizes the peak acceleration needed to move from one cam point to another.

This can be useful when the motors cannot support the accelerations used by other segment types.

Disadvantages

Acceleration is discontinuous which can lead to additional electrical stress on the drives and motors.

Point Segment Type

Segment Curve

Velocity

Acceleration

Jerk

Supported by

KAS-IDE Profile Editor

MLProfileBuild (default option)

Continuous Velocity

Continuous Acceleration

Interpolation Method

5th order polynomial: f(x) = Ax5 + Bx4 + Cx3 + Dx2 + Ex + F

Advantages

With only a few segments, this type can be used to define profiles with continuously changing accelerations.

Example: Sinusoidal profiles can be emulated with 6 to 12 point segments.

Disadvantages

Specify the velocity and acceleration at the endpoints for each segment.

It is difficult to use the point segment type to define constant acceleration or constant velocity segments.

Spline Segment Type

Segment Curve

Velocity

Acceleration

Jerk

Supported by

KAS-IDE Profile Import.

The points are created by separate software and is imported into KAS-IDE project.

Continuous Velocity

Continuous Acceleration

Interpolation Method

3rd order polynomial: f(x) = Ax3 + Bx2 + Cx + D

Advantages

With only a few segments, this segment type can be used to define profiles with continuously changing velocities.

Only the positions of the master and slave need to be specified.

This produces smoother profiles than using line segments.

Disadvantages

Since only positions are specified, the user has less control over the velocities and accelerations that occur throughout the profile.