FSoE / PDO Connections tab

The Fail Safe over EtherCAT (FSoE) tab displays devices discovered on the EtherCAT network, listing their Input (Tx) and Output (Rx) PDOs.

This provides you with a way to connect an Input PDO to an Output PDO.

The KAS Runtime copies the PDO data between the connected PDOs when EtherCAT is in operational mode. This feature makes it possible to transfer safety-critical process data via the EtherCAT frames. The FSoE protocol, communication, and state machine are handled by the EtherCAT Safety devices.


  • Connected PDOs are intended for FSoE operation.
    This feature is not limited to FSoE, it could be useful for any application that need to copy PDO data between EtherCAT devices.


  • Inputs and Outputs must have identical Bit sizes in order to be paired.

See Also

Safety over EtherCAT