Intellisense

The following features are available with Intellisense in ST and FBD programs:


  • They do not apply to actions in an SFC step.

Conditional compiling coloring

Parts of conditional compiling code (declared with #ifdef pragmas) that are not validated are grayed

Commenting the CONDITION changes the active part of the program


  • Save your project to have the code with the correct colors.

Auto-indentation

Lines are automatically indented on the left when you enter structured ST statements

Autocompletion