AKD PDMM and PCMM - File Naming Conventions

AKD PDMM and PCMM use only .IMG files.

File Contents

This .IMG file contains the Operating System (OS) and the KAS Runtime (RT) software.

Usage

The contents of this .IMG file are used to update the AKD PDMM and PCMM from the web server interface.

File Format and Examples

AKD PDMM

Controller

File Name Format

Example File Name

AKD PDMM

KAS-PDMM-M-{Model-Code}-{Software-Version}.img
KAS-PDMM-M-K1EC-4.01.0.91992.img

PCMM

Controller

File Name Format

Example File Name

PCMM

KAS-PCMM-M-{Model-Code}-{Software-Version}.img
KAS-PCMM-M-M2EC-4.01.0.91992.img

Model Code

This table shows the specified model's CPU speed and number of cores.

Model Code

CPU Speed

Core

KCEC and MCEC

800 MHz

Single

K1EC and M1EC

1.2 GHz

Single

M2EC

1.2 GHz

Dual

See Also