AKD PDMM or PCMM Controller Backup
This function is used to replicate a PCMM or the controller portion of the AKD PDMM.
Click the button to save the data to the SD card.
- The 1.2GHz single core Runtime firmware file is optional.
- If the 1.2GHz single core Runtime firmware file is not included, an 800MHz single core model can only be replaced with another 800MHz single core model.
- If provided, an 800MHz single core model can be replaced with a 1.2GHz single core model.
After starting, a confirmation message opens to confirm the backup.
Click OK to continue.
See Also