Home tab

To access the KAS web server home page, enter the controller's IP address.

This page provides an overview of the device including:

  • Manufacturer
  • CPU Speed
  • CPU Cores
  • Model Number
  • Serial Number
  • Hardware Revision
  • TCP/IP MAC Address — a unique value associated with the TCP/IP network adapter that uniquely identifies the adapter on a LAN.
  • EtherCAT MAC Address — a unique value associated with the EtherCAT network adapter that uniquely identifies the adapter on an EtherCAT network.

  • Unless otherwise noted, any reference to AKD PDMM or PCMM refers to both the 800MHz and the single- and dual-core 1.2GHz variants.