WorkBench 2 in the KAS-IDE

WorkBench 2 views are integrated into the KAS-IDE, and are accessible from the AKD or AKD2G drive's Configuration tab when the controller is started or in Online Configuration mode.

AKD and AKD2G device views may be different than each other because the devices have different capabilities.


  • To save resources and minimize the time it takes to open a project, the state of AKD views is not saved.
    Views need to be opened each time a project is opened.