Map Variables to the Control Panel
To map the variable:
- Select the variable in the Dictionary toolbox
- Move it to the control to be linked in the Control panel editor using drag-and-drop

Figure 2: Map Variables to a Control Panel Control in the Graphical Editor
The Variable symbol is automatically updated in the Properties tab.
-
-
A warning will be generated when the program is compiled if the control is mapped to a variable which is not in the Dictionary. Double-clicking the warning will highlight the control object and open the editor so the variable can be defined.