Setting Scale

The soft oscilloscope graph is divided into eight units for the horizontal time scale (X-axis) and eight units for the amplitude (Y-axis). These units can be user-defined by using the configuration panels described below.


  • Unit per ulision: This is the time-base value for the X-axis and to the amplitude value for the Y-axis.
    Example: If the user sets a time-base of 10ms and an amplitude of 1, each ulision in the soft oscilloscope grid corresponds to a time of 10ms for the X-axis and an amplitude of 1 for the Y-axis.

Time Scale

Variable Scale