Structures
All the structures within the entire system project are grouped as follows:
Description |
|
EtherCATCode |
List all the devices as PLC variables so you can use their names in FBs instance See example here
• The devices are displayed under the EtherCAT node in the Project Explorer (see call out ) • The same devices are also displayed as PLC variables in the Dictionary • You can use them in your PLC programs with a drag-and-drop operation
|
PNCode |
List all the variables related to the specific Pipe Network Code |
ProfilesCode |
List all the variables related to the specific profiles |
PLCopenCode |
List all the variables related to the specific PLCopen Code |
UDFB variables |
List the variables related to a specific UDFB |