AXIS#.IL.AINSOURCE
Description
This parameter sets which analog input to use for AXIS#.IL.AINSCALE.
| Value | Description |
|---|---|
| 0 | Uses no analog input. The current command in analog torque mode is 0. |
| 1 | Uses AIN1 |
| 2 | Uses AIN2 |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
| Added value '0' to range | 02-07-02-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 2 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.IL.AINSOURCE |
500ah |
15h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
AXIS2.IL.AINSOURCE |
510ah |
15h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
AXIS1.IL.AINSOURCE |
5811 |
16B3 |
Unsigned8 |
Read/Write |
- |
|
AXIS2.IL.AINSOURCE |
71347 |
116B |
Unsigned8 |
Read/Write |
- |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.IL.AINSOURCE |
5811 |
Unsigned8 |
Read/Write |
- |