AXIS#.MOTOR.RTYPE

Description

This parameter defines the type of thermal resistor inside the motor to measure motor temperature. The following resistor types are supported:

AXIS#.MOTOR.RTYPE Thermal Resistor Type
0 Single PTC
1 Single NTC
2 KTY83-110
3 KTY84-130
4 PTC + KTY83-110
5 Thermal switch
6 PTC + PT1000
7 Dual PTC
8 PT1000
127 No sensor

See Motor Temperature View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 8, 127

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.RTYPE

500bh

19h

Unsigned8

-

-

Read/Write

No

AXIS2.MOTOR.RTYPE

510bh

19h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.RTYPE

6214

1846

Unsigned8

Read Only

-

AXIS2.MOTOR.RTYPE

71750

1184

Unsigned8

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.RTYPE

6214

Unsigned8

Read Only

-