AXIS#.PL.KFB
Refer to AXIS#.PL.KFB.PIN for details.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-08-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | - 2,147,483,648 to 2,147,483,647 |
| Default Value | 1.0 |
| Data Type | Float |
| See Also | AXIS#.PL.KFB.PIN, AXIS#.PL.KFB.POUT |
| Stored in Non-Volatile Memory | Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.PL.KFB |
500ch |
0dh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
AXIS2.PL.KFB |
510ch |
0dh |
Signed32 |
- |
1000:1 |
Read/Write |
No |