AXIS#.PROFINET.​ACTUALVALUEMAP

Description

This command specifies which signals are currently mapped to the actual value telegram of the axis. If using a pre-defined telegram, it is read only and displays the mapped signals. If telegram 0 is selected, it is writable if the PROFIdrive state (AXIS#.PROFINET.STATE) is in the shutdown state.

Only signals available in AXIS#.PROFINET.SIGNALLIST labeled as actual values are allowed to be written and the first index is required to be the statusword, signal 2 ZSW1.

See Telegram Configuration.

Example

-->AXIS1.PROFINET.SETPOINTMAP

[0] 2

[1] 6

[2] 0

[3] 0

[4] 0

[5] 0

[6] 0

[7] 0

[8] 0

[9] 0

[10] 0

[11] 0

[12] 0

[13] 0

[14] 0

[15] 0

Versions

Action Version Notes
Implemented 02-04-05-000  

General Information

Type Read/Write
Units

N/A

Range 0 to 65535
Default Value 0 - Unmapped
Data Type Integer
Stored in Non-Volatile Memory Yes

Variants Supported

PROFINET drives: AKD2G-SPP

Fieldbus Information

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PROFINET.ACTUALVALUEMAP

916

Unsigned16[16]

Read Only

-