CMP#.WIDTHT
Description
CMP#.WIDTHT sets the time duration of the output pulse generated by the setpoint. It is used when CMP#.WIDTHTYPE for the setpoint is set to 1.
It takes two command line arguments: the first specifies the setpoint, and the second specifies the time duration.
Examples
The following diagram illustrates CMP#.WIDTHT
.
Code
The following commands set the time widths of channel 1 setpoint 5 to 3.5 ms and channel 2 setpoint 1 to 20 ms.
--> CMP1.WIDTHTYPE 5 1
--> CMP1.WIDTHT 5 3.5
--> CMP2.WIDTHTYPE 1 1
--> CMP2.WIDTHT 1 20
Context
For more information please refer to Compare.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-06-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
ms |
|
Range |
0 to 1000.000 |
|
Default Value |
0 |
|
Data Type |
Float |
|
See Also |
|
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
CMP1.WIDTHT |
31460 |
7AE4 |
Unsigned32[8] |
Read/Write |
- |
|
CMP2.WIDTHT |
31461 |
7AE5 |
Unsigned32[8] |
Read/Write |
- |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
CMP1.WIDTHT |
31460 |
Float[8] |
Read/Write |
- |
|
CMP2.WIDTHT |
31461 |
Float[8] |
Read/Write |
- |