CMP#.WIDTHVAL
Description
CMP#.WIDTHVAL sets the value count duration of the output pulse generated by the setpoint. It is used when CMP#.WIDTHTYPE for the setpoint is set to 0. Its scaling depends on CMP#.SOURCE.
It takes two command line arguments: the first specifies the setpoint, and the second specifies the value count duration.
Examples
The following diagram illustrates CMP#.WIDTHVAL.
Code
The following commands set the value count widths of channel 1 setpoint 8 to 5 deg and channel 2 setpoint 6 to 4000000 (slightly less than one thousandth of a revolution).
--> CMP1.SOURCE 11
--> AXIS1.UNIT.PROTARY 2
--> CMP1.WIDTHTYPE 8 0
--> CMP2.WIDTHVAL 8 5
--> CMP2.SOURCE 2
--> CMP2.WIDTHTYPE 6 0
--> CMP2.WIDTHVAL 6 4000000
Context
For more information please refer to Compare.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-06-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Depends upon CMP#.SOURCE |
|
Range |
Full position range |
|
Default Value |
0 |
|
Data Type |
Float |
|
See Also |
|
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
CMP1.WIDTHVAL |
31500 |
7B0C |
Signed32[8] |
Read/Write |
Position |
|
CMP2.WIDTHVAL |
31501 |
7B0D |
Signed32[8] |
Read/Write |
Position |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
CMP1.WIDTHVAL |
31500 |
Signed32[8] |
Read/Write |
Position |
|
CMP2.WIDTHVAL |
31501 |
Signed32[8] |
Read/Write |
Position |