DRV.FAULTS
Description
Indicates what faults are present on the drive regardless of axis. For axis specific faults, see AXIS#.FAULTS.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type | Read Only |
Units | N/A |
Range | N/A |
Default Value | N/A |
Data Type | String |
Stored in Non-Volatile Memory |
No |
Variants Supported
Supported on all device types.