EEO#.PIN
Description
EEO#.PIN is used in conjunction with EEO#.POUT to set the gain of the EEO position going to the EEO Generator. The maximum value of EEO#.PIN / EEO#.POUT is 32.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-07-00-000 |
General Information
| Type | Read/Write |
| Description | Sets the gear IN of the EEO position |
| Units | N/A |
| Range | 1 to 4,294,967,295 |
| Default Value | 1 |
| Data Type | Integer |
| See Also | EEO#.POUT |
| Stored in Non-Volatile Memory | Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
EEO1.PIN |
4600h |
08h |
Unsigned32 |
- |
- |
Read/Write |
No |
|
EEO2.PIN |
4601h |
08h |
Unsigned32 |
- |
- |
Read/Write |
No |
|
EEO3.PIN |
4603h |
08h |
Unsigned32 |
- |
- |
Read/Write |
No |
|
EEO4.PIN |
4606h |
08h |
Unsigned32 |
- |
- |
Read/Write |
No |
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
EEO1.PIN |
32045 |
7D2D |
Unsigned32 |
Read/Write |
- |
|
EEO2.PIN |
32046 |
7D2E |
Unsigned32 |
Read/Write |
- |
|
EEO3.PIN |
32047 |
7D2F |
Unsigned32 |
Read/Write |
- |
|
EEO4.PIN |
32048 |
7D30 |
Unsigned32 |
Read/Write |
- |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
EEO1.PIN |
32045 |
Unsigned32 |
Read/Write |
- |
|
EEO2.PIN |
32046 |
Unsigned32 |
Read/Write |
- |
|
EEO3.PIN |
32047 |
Unsigned32 |
Read/Write |
- |
|
EEO4.PIN |
32048 |
Unsigned32 |
Read/Write |
- |