FB#.P
Description
This parameter is the 64 bit position of the feedback device. The position is given in counts. The parameter takes actual feedback position (with resolution specified in FB#.RES ) and converts it into a format of 32:32.
-
For rotary feedback, the upper 32 bits represent the number of motor turns and the lower 32 bits represent the position within one turn.
-
For linear feedback, the upper 32 bits represent the number of motor pole-pairs and the lower 32 bits represent the position within one pole-pair distance of the motor.
Example
Rotary feedback position = 542,456,123,450 or 0111 1110 0100 1100 1110 0111 1001 0000 0011 1010 binary
Number of turns = 0111 1110 binary or 126 decimal
Position within a turn = 0100 1100 1110 0111 1001 0000 0011 1010 binary or 1,290,244,154 decimal
Context
See Feedback # View.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
Counts |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
FB1.P |
30240 |
7620 |
Signed32 |
Read Only |
Position |
|
FB2.P |
30241 |
7621 |
Signed32 |
Read Only |
Position |
|
FB3.P |
30242 |
7622 |
Signed32 |
Read Only |
Position |
|
FB4.P |
30243 |
7623 |
Signed32 |
Read Only |
Position |
|
FB5.P |
30244 |
7624 |
Signed32 |
Read Only |
Position |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
FB1.P |
30240 |
Signed32 |
Read Only |
Position |
|
FB2.P |
30241 |
Signed32 |
Read Only |
Position |
|
FB3.P |
30242 |
Signed32 |
Read Only |
Position |
|
FB4.P |
30243 |
Signed32 |
Read Only |
Position |
|
FB5.P |
30244 |
Signed32 |
Read Only |
Position |