PWM#.DUTYCYCLE
Description
Sets the duty cycle of the PWM signal, that can be output on a digital IO with DIO#.SOURCE 6.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-11-03-000 |
General Information
| Type | Read/Write |
| Units | Percent |
| Range | 0.0 to 100.0 |
| Default Value | 0.0 |
| Data Type | Float |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported