PWM#.PERIOD
Description
Sets the period length of the PWM signal, that can be output on a digital IO with DIO#.SOURCE 6.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-11-03-000 |
General Information
| Type | Read/Write |
| Units | Microseconds |
| Range | 1 to 500 |
| Default Value | 1 |
| Data Type | Integer |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported