REGEN.POWER
Description
This parameter reads regen resistor's calculated power, which is determined as follows:
(V2 / R) * DutyCycle
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
Watt |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
REGEN.POWER |
3007h |
02h |
Unsigned32 |
- |
- |
Read only |
Yes |
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
REGEN.POWER |
2400 |
960 |
Unsigned32 |
Read Only |
- |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
REGEN.POWER |
2400 |
Unsigned32 |
Read Only |
- |