REGEN.TYPE

Description

You can specify a user-defined external regen resistor or select the internal regen resistor. The values for REGEN.TYPE are shown below:

Type

Option

Description

–1

External Regen

External user-defined regen resistor

0

Internal Regen (if available)

Internal regen resistor

If a user-defined regen resistor is specified, then you must also define this resistor's resistance (REGEN.REXT ), heatup time (REGEN.TEXT ), and power (REGEN.WATTEXT ).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

–1 to 0

Default Value

0

Data Type

Integer

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

REGEN.TYPE

3007h

03h

Signed8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

REGEN.TYPE

2403

963

Signed8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

REGEN.TYPE

2403

Signed8

Read/Write

-